How to WiFi: Configuring the WINC1500 driver with the Harmony 3 Configurator

How to WiFi: Configuring the WINC1500 driver with the Harmony 3 Configurator

This is a short tutorial showing how to use the Harmony 3 Configurator to configure the WINC1500 driver from scratch in a new project. (Jan 2022)

rate limit

Code not recognized.

About this course

This is a short tutorial showing how to use the Harmony 3 Configurator to configure the WINC1500 driver from scratch in a new project. It explains the hardware interface the WINC1500 employs, shows how to determine which MCU pins and peripherals are leveraged based on the schematic design, and then demonstrates using the Harmony 3 configurator to adjust the WINC1500 driver settings. The configuration will include all the supporting services, peripherals and pins that are needed to use the WINC1500 module.

The concepts taught in this training are helpful for developers that want to bring up a new board featuring a WINC1500, add a WINC1500 to an existing project, or modify an existing WINC1500 project to accommodate system level hardware changes.

 

Curriculum32 min

  • Syllabus
  • Course Introduction 2 min
  • MPLAB® Development Toolchain
  • Toolchain 2 min
  • Harmony 3 Content Manager 4 min
  • WINC1500 Firmware and Hardware Architecture
  • Hardware/Firmware Overview 6 min
  • Configuring the WINC Drivers and Services
  • Creating a New Harmony Project 2 min
  • Project Configuration 5 min
  • Pin Configuration 3 min
  • Testing and Debugging
  • Building and Testing the Project 3 min
  • Debugging Tips 5 min
  • Your Feedback
  • We need your Feedback

About this course

This is a short tutorial showing how to use the Harmony 3 Configurator to configure the WINC1500 driver from scratch in a new project. It explains the hardware interface the WINC1500 employs, shows how to determine which MCU pins and peripherals are leveraged based on the schematic design, and then demonstrates using the Harmony 3 configurator to adjust the WINC1500 driver settings. The configuration will include all the supporting services, peripherals and pins that are needed to use the WINC1500 module.

The concepts taught in this training are helpful for developers that want to bring up a new board featuring a WINC1500, add a WINC1500 to an existing project, or modify an existing WINC1500 project to accommodate system level hardware changes.

 

Curriculum32 min

  • Syllabus
  • Course Introduction 2 min
  • MPLAB® Development Toolchain
  • Toolchain 2 min
  • Harmony 3 Content Manager 4 min
  • WINC1500 Firmware and Hardware Architecture
  • Hardware/Firmware Overview 6 min
  • Configuring the WINC Drivers and Services
  • Creating a New Harmony Project 2 min
  • Project Configuration 5 min
  • Pin Configuration 3 min
  • Testing and Debugging
  • Building and Testing the Project 3 min
  • Debugging Tips 5 min
  • Your Feedback
  • We need your Feedback